• AVR Freaks

Hot!chargin IO - MCP73832T-2DFI/OT - DF meaning

Author
lupal
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2008/02/10 09:31:47
  • Location: 0
  • Status: offline
2020/01/20 00:01:02 (permalink)
0

chargin IO - MCP73832T-2DFI/OT - DF meaning

Hi all,
I would like to find out what DF stands for in MCP73832T-2DFI/OT component type.
Datasheet does not mention it.
Does anyone have experience with it?
Thank you.
 
#1

3 Replies Related Threads

    ric
    Super Member
    • Total Posts : 25502
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: chargin IO - MCP73832T-2DFI/OT - DF meaning 2020/01/20 00:32:29 (permalink)
    0
    lupal
    I would like to find out what DF stands for in MCP73832T-2DFI/OT component type.
    Datasheet does not mention it.

    The datasheet does mention four options (AC, AD, AT, DT), but not "DF" as you say.
    However, it goes on to say "* Consult Factory for Alternative Device Options", so plainly this is another custom alternative.
    Where did you see it?
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    1and0
    Access is Denied
    • Total Posts : 10299
    • Reward points : 0
    • Joined: 2007/05/06 12:03:20
    • Location: Harry's Gray Matter
    • Status: offline
    Re: chargin IO - MCP73832T-2DFI/OT - DF meaning 2020/01/20 05:07:10 (permalink)
    0
    ric
     
    The datasheet does mention four options (AC, AD, AT, DT), but not "DF" as you say.
    However, it goes on to say "* Consult Factory for Alternative Device Options", so plainly this is another custom alternative.
    Where did you see it?

    Page 19 lists AC, AD, AT, DC, and DF.  
     
    http://ww1.microchip.com/downloads/en/DeviceDoc/20001984g.pdf
     
    #3
    ric
    Super Member
    • Total Posts : 25502
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: chargin IO - MCP73832T-2DFI/OT - DF meaning 2020/01/20 12:12:27 (permalink)
    0
    So it does. They forgot to update page 25 to explain what it means.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5