• AVR Freaks

AnsweredHot!OSX Catalina patch - just MPLABX or also the compilers?

Author
j2423
Super Member
  • Total Posts : 283
  • Reward points : 0
  • Joined: 2015/05/15 23:10:36
  • Location: 0
  • Status: offline
2020/01/01 06:53:48 (permalink)
0

OSX Catalina patch - just MPLABX or also the compilers?

Just note the existence of an OSX Catalina patch.
 
Does this enable compilers (notably XC8) to run with MPLABX on Catalina?
#1
rjc101
Super Member
  • Total Posts : 133
  • Reward points : 0
  • Joined: 2016/07/08 14:56:34
  • Location: 0
  • Status: offline
Re: OSX Catalina patch - just MPLABX or also the compilers? 2020/01/01 12:18:44 (permalink) ☼ Best Answerby j2423 2020/01/01 21:49:49
+1 (1)
Just tested an 8-bit app on MPLAB 5.30 under Catalina, all OK with the patch.  However XC16 and XC32 still require an update to work.
#2
agha
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2020/01/01 14:59:11
  • Location: 0
  • Status: offline
Re: OSX Catalina patch - just MPLABX or also the compilers? 2020/01/03 07:26:36 (permalink)
0
I cant install MPLAB X IDE 5.30 in macOS Catalina 10.15.2 with patch or without patch.
Do you know what problem is?
post edited by agha - 2020/01/05 11:16:38
#3
rjc101
Super Member
  • Total Posts : 133
  • Reward points : 0
  • Joined: 2016/07/08 14:56:34
  • Location: 0
  • Status: offline
Re: OSX Catalina patch - just MPLABX or also the compilers? 2020/01/06 11:07:52 (permalink) ☄ Helpfulby agha 2020/01/06 14:33:27
+3 (3)
agha
I cant install MPLAB X IDE 5.30 in macOS Catalina 10.15.2 with patch or without patch.
Do you know what problem is?


The Mac download is a .dmg, open that you will see the installer.  Don't double click it, but right click it and select Open.  The in the next warning box you can select to Open the installer, you will be asked to enter your machine password and then the installer will run.
 
The installer doesn't appear to be signed with an Apple certificate, hence the double click will fail.  The right click let you override this with the Open button.
 
You may have to do this with the patch too.
#4
agha
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2020/01/01 14:59:11
  • Location: 0
  • Status: offline
Re: OSX Catalina patch - just MPLABX or also the compilers? 2020/01/06 14:34:06 (permalink)
0
Thank you for helping!
it works!Smile: Smile
#5
Jump to:
© 2020 APG vNext Commercial Version 4.5