• AVR Freaks

Hot!MRF24WG module

Author
tcross
Super Member
  • Total Posts : 287
  • Reward points : 0
  • Joined: 2006/09/09 07:57:22
  • Location: 0
  • Status: offline
2019/12/31 22:51:13 (permalink)
0

MRF24WG module

Hi All
 I have a MRF24wg module plugged into a Explorer 16/32 board. I am using demo code "XC32_EX16_MRF24WG" from MLA V2012_08_12. It all seems to work as I am getting blinking LEDs on the Explorer board and also serial output as  shown below. The question is shouldn't I be seeing the MicrochipDemoAP on my wireless networks? I am not completely sure what I should be seeing.......
 
*** WiFi TCP/IP Demo ***
Start WiFi Connect
Domain: FCC
MAC: 00 1E C0 1A 3E 7D
SSID: MicrochipDemoAP
Network Type: Infrastructure
Scan Type: Active Scan
Channel List: 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11
Retry Count: Retry Forever
Beacon Timeout: 40
Security: Open
Power Save: Disabled
New IP Address: 192.168.1.10
 
Thanks for reading
 
 
#1

2 Replies Related Threads

    diego3602
    New Member
    • Total Posts : 24
    • Reward points : 0
    • Joined: 2018/11/25 16:47:59
    • Location: 0
    • Status: offline
    Re: MRF24WG module 2020/02/28 07:13:42 (permalink)
    0
    Network-type is infrastructure. No esta como Ad-hoc. deberias de verla como dispositivo en tu router no como red.
     
    prueba cambiar MY_DEFAULT_NETWORK_TYPE to CFG_WF_ADHOC
    #2
    diego3602
    New Member
    • Total Posts : 24
    • Reward points : 0
    • Joined: 2018/11/25 16:47:59
    • Location: 0
    • Status: offline
    Re: MRF24WG module 2020/02/28 07:16:44 (permalink)
    0
    retry count value no deberia ser retry_forever en otro ejemplo le asigna el valor de 3. fijate en Wifi EZ_config folder ahi tienes un ejemplo para usar la placa como red ad-hoc y poder escanear redes y conectarte a una de tipo infraestructura.
     
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5