• AVR Freaks

PGEC & PGED pin configuration

Author
ashvin
New Member
  • Total Posts : 13
  • Reward points : 0
  • Joined: 2019/11/18 03:59:01
  • Location: 0
  • Status: offline
2019/12/25 02:12:16 (permalink)
0

PGEC & PGED pin configuration

Hello,
my question is that in dsPIC33F family micro controller, how to used PGEC and PGED pin as debugging?
#1

1 Reply Related Threads

    ric
    Super Member
    • Total Posts : 25244
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: PGEC & PGED pin configuration 2019/12/25 02:14:06 (permalink)
    5 (1)
    Which particular dsPIC33F?
     
    I'll make an educated guess you're interested in a dsPIC33FJ16GS504
    That has PGEx1, PGEx2 and PGEx3 pairs of pins.
    You must specify which pair to use in your PIC's CONFIG settings. That is via the "ICS" bits in the FICD register.
    Programming can be via any pair, but debugging will only work via the specified pair.
     
    post edited by ric - 2019/12/25 02:27:43

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5