• AVR Freaks

LockedHot!Tatalina

Author
horkesley
Super Member
  • Total Posts : 285
  • Reward points : 0
  • Joined: 2008/09/09 00:13:17
  • Location: Essex,UK
  • Status: offline
2019/12/14 11:02:46 (permalink)
0

Tatalina

So, MPLABX will run on a MAC with Catalina OS.
 
But, there is no compiler?
 
Have I got this correct.
 
Regards
#1

3 Replies Related Threads

    JasonK
    Moderator
    • Total Posts : 3411
    • Reward points : 0
    • Joined: 2003/11/14 09:49:40
    • Location: Microchip Technology in Arizona, USA
    • Status: offline
    Re: Tatalina 2019/12/14 16:22:23 (permalink)
    +2 (2)
    MPLAB XC8 works on Catalina now. The next XC16 and XC32 releases are in validation now. We expect them to be released early next year.

    For XC32, we identified a problem in the PIC32M (MIPS) assembler related to the 64-bit Catalina change and need to get that fixed and validated first.

    Thanks for the patience!

    Jason Kajita
     Follow me on Twitter
    http://support.microchip.com for urgent questions
    #2
    katela
    Super Member
    • Total Posts : 1830
    • Reward points : 0
    • Joined: 2013/06/11 05:25:18
    • Location: South Africa
    • Status: offline
    Re: Tatalina 2019/12/14 16:25:07 (permalink)
    0
    There is also XC8 Compilers for MAC check the release notes if it runs on catalina
    post edited by katela - 2019/12/14 16:28:06

    Free online Microcontroller Tutorials and Projects for Hobbyists and students. From beginners to advanced. Website: www.studentcompanion.co.za
    YouTube Tutorials: https://www.youtube.com/StudentCompanionSA
    #3
    horkesley
    Super Member
    • Total Posts : 285
    • Reward points : 0
    • Joined: 2008/09/09 00:13:17
    • Location: Essex,UK
    • Status: offline
    Re: Tatalina 2019/12/14 23:09:52 (permalink)
    0
    Thanks for the replies.
     
    Unfortunately I require XC32 for PIC32MX, so I will wait.
     
    Regards
     
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5