• AVR Freaks

Hot!MPLAB Harmony Build Issue

Author
AlbinCaliber@
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2019/11/28 21:05:33
  • Location: 0
  • Status: offline
2019/12/13 22:33:50 (permalink)
5 (1)

MPLAB Harmony Build Issue

Hi sir/Madam,
                        I was trying to build a simple UART program for SAM9X60 Microprocessor using MPLAB Harmony(version 5.30,XC32 compiler). But i ended up with cstartup.s and vectortrap.s file error. I attached the error below following.
                       Note: Same program i tried for SAMAD23 Microprocessor, it's buid successfully.
Error
make -f nbproject/Makefile-default.mk SUBPROJECTS= .build-conf
../src/config/default/vectortrap.s: Assembler messages:
../src/config/default/vectortrap.s:24: Error: bad instruction `module ?vectortrap'
../src/config/default/vectortrap.s:28: Error: bad instruction `pubweak undefined_instruction_irq_handler'
../src/config/default/vectortrap.s:29: Error: bad instruction `pubweak software_interrupt_irq_handler'
../src/config/default/vectortrap.s:30: Error: bad instruction `pubweak prefetch_abort_irq_handler'
../src/config/default/vectortrap.s:31: Error: bad instruction `pubweak data_abort_irq_handler'
../src/config/default/vectortrap.s:33: Error: bad instruction `section .text:CODE:NOROOT:REORDER(2)'
../src/config/default/vectortrap.s:34: Error: bad instruction `arm'
../src/config/default/vectortrap.s:36: Error: bad instruction `call_graph_root __default_handler,"interrupt"'
../src/config/default/vectortrap.s:37: Error: bad instruction `nocall __default_handler'
../src/config/default/vectortrap.s:47: Error: bad instruction `end'
make[2]: *** [build/default/production/_ext/1171490990/vectortrap.o] Error 1
make[2]: *** Waiting for unfinished jobs....
make[1]: Entering directory '/home/cis-113/HarmonyProjects/MyProject_3/firmware/UART.X'
make  -f nbproject/Makefile-default.mk dist/default/production/UART.X.production.hex
make[2]: Entering directory '/home/cis-113/HarmonyProjects/MyProject_3/firmware/UART.X'
.
.
Thank You
post edited by AlbinCaliber@ - 2019/12/15 21:51:30
#1

2 Replies Related Threads

    arpananand
    Super Member
    • Total Posts : 488
    • Reward points : 0
    • Joined: 2009/11/18 04:35:42
    • Location: 0
    • Status: offline
    Re: MPLAB Harmony Build Issue 2019/12/18 21:41:40 (permalink)
    0
    The released MPLAB X IDE v5.30 with MPLAB XC32/32++ Compiler v2.30 is not supporting SAM9X60 device.
     
    The next release of MPLAB X IDE and XC32 compiler will support SAM9X60 device.
    #2
    AlbinCaliber@
    New Member
    • Total Posts : 6
    • Reward points : 0
    • Joined: 2019/11/28 21:05:33
    • Location: 0
    • Status: offline
    Re: MPLAB Harmony Build Issue 2019/12/18 22:21:06 (permalink)
    0
    Thank You for your response arpanand.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5