• AVR Freaks

Hot!USB communication with LORA Gateway core board.

Author
Doug Richard
Super Member
  • Total Posts : 263
  • Reward points : 0
  • Joined: 2003/11/07 12:42:00
  • Status: offline
2019/12/13 14:12:49 (permalink)
0

USB communication with LORA Gateway core board.

Hi.  Trying to connect LoRa development utility program to my gateway board.  I click find devices and can see the command requesting the device version make it to the board.  However I see no response from the board to this message.
 
Using the same application I can connect to the Mote boards.
 
Anyone else have this issue?
 
Doug.

Doug Richard
= != ==
#1

1 Reply Related Threads

    Doug Richard
    Super Member
    • Total Posts : 263
    • Reward points : 0
    • Joined: 2003/11/07 12:42:00
    • Status: offline
    Re: USB communication with LORA Gateway core board. 2019/12/17 08:17:29 (permalink)
    5 (1)
    Reached out to tech support.  Standard re flash did not help.

    Doug Richard
    = != ==
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5