• AVR Freaks

Hot!MAC OS Catalina 10.15 support patch

Author
DevMod1
Administrator
  • Total Posts : 545
  • Reward points : 0
  • Joined: 2009/02/10 09:34:30
  • Location: 0
  • Status: offline
2019/12/11 10:26:26 (permalink)
5 (1)

MAC OS Catalina 10.15 support patch

We've just released a patch to allow macOS users to run MPLAB X IDE with Catalina 10.15 (removed 32-bit applications). The patch can be found on the MPLAB X IDE page, under the "Java® Platform and Operating System Direction" section here: https://www.microchip.com/mplab/mplab-x-ide
 
This patch is only needed for MPLAB X 5.30 and older.  The MPLAB X v5.35 does not need this patch.
post edited by DevMod1 - 2020/03/03 08:22:49

_____________________________

Please read the forum posting guidelines. Do not double post, please help keep these forums professional and comments respectful.
Please notify the moderators of problems/spam/trolls.
#1

14 Replies Related Threads

    agha
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2020/01/01 14:59:11
    • Location: 0
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2020/01/03 07:25:00 (permalink)
    -1 (1)
    I cant install MPLAB X IDE 5.30 in macOS Catalina 10.15.2 with patch or without patch.
    Can you know what problem is?
    #2
    ric
    Super Member
    • Total Posts : 30285
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: MAC OS Catalina 10.15 support patch 2020/01/06 12:37:13 (permalink)
    +1 (1)
    agha
    I cant install MPLAB X IDE 5.30 in macOS Catalina 10.15.2 with patch or without patch.
    Can you know what problem is?

    https://www.microchip.com/forums/m1123391.aspx
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #3
    dobrosoft
    Junior Member
    • Total Posts : 114
    • Reward points : 0
    • Joined: 2019/05/20 04:44:55
    • Location: 0
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2020/02/14 08:12:01 (permalink)
    +1 (1)
    On your webpage with patch download link is wrotten:
    Important Note for macOS® Users: The latest version of macOS, 10.15 Catalina, removes support for 32-bit applications. This means that current versions of MPLAB X IDE (up to version 5.40) will not run on this operating system without a patch. While this patch allows for MPLAB X IDE to be compatible with the Catalina update, only the MPLAB XC8 compiler is currently compatible. The MPLAB XC16 and MPLAB XC32 compilers will be updated for compatibility in January.
     
    I need use XC32, and I didn't update to Catalina yet, because it is still incompatible. Update is important for me, because I develop for 
    Xcode too, and it needs Catalina. When Will be fixed XC16 and XC32. 
     
    #4
    mpgmike
    Super Member
    • Total Posts : 542
    • Reward points : 0
    • Joined: 2014/01/23 17:27:06
    • Location: NJ
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2020/02/14 09:30:34 (permalink)
    +1 (1)
    XC16 v1.50 (current version) is 64-bit.  Still waiting on XC32.

    I don't need the world to know my name, but I want to live a life so all my great-grandchildren proudly remember me.
    #5
    tansik
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2020/01/07 05:34:14
    • Location: 0
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2020/02/29 12:34:23 (permalink)
    0
    .
    post edited by tansik - 2021/01/29 15:47:49
    #6
    ric
    Super Member
    • Total Posts : 30285
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: MAC OS Catalina 10.15 support patch 2020/03/02 11:59:20 (permalink)
    +1 (1)
    tansik
    Hello!
     
    I applied the patch, but I still get this erros when assembling.
    Could anybody help me please ?
     
    sh: /Applications/microchip/mplabx/v5.30/mpasmx/mpasmx: Bad CPU type in executable
    make[2]: *** [nbproject/Makefile-default.mk:111: build/default/production/newpic_8b_general.o] Error 1
    make[1]: *** [nbproject/Makefile-default.mk:91: .build-conf] Error 2
    make: *** [nbproject/Makefile-impl.mk:39: .build-impl] Error 2

    What PIC are you compiling for?
    Which compiler version are you using?
     




    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #7
    cty
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2020/03/27 09:02:20
    • Location: 0
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2020/04/03 02:53:14 (permalink)
    0
    Hi,
     
    I am using Mac with Catalina 10.15.4 and MPLAB IDE v5.35. However I still receive the message "MPASM is not supported on 64 bit Operating Systems." and when I try to build project, it always gives me "sh: /Applications/microchip/mplabx/v5.35/mpasmx/mpasmx: Bad CPU type in executable". I also tried older version IDE with the patch, but still doesn't work.
     
    I am using PIC16F887 and MPASMWIN(v5.87). Please help me with this issue. Many thanks!
    #8
    g1l1t1
    Starting Member
    • Total Posts : 23
    • Reward points : 0
    • Joined: 2020/02/27 06:19:02
    • Location: 0
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2020/04/07 11:56:17 (permalink)
    0
    I tried to use the 64 bit release on MacOS High Sierra (10.13), but the make that is supplied with it was linked on a later release of MacOS and doesn't work on High Sierra.
     
    A simple fix:
    1. Go to mplabx/v5.35/mplab_platform/bin
    2. [Optional, but safest] Rename or stash away a backup copy of the make that you find there.
    3. In the same folder, create a soft link, also named make, to a version of that tool that works on your system. I used gnu make which I had installed (using brew) at /usr/local/bin/gmake but you could probably just use the one at /usr/bin/make.
    Gnu make worked fine for me.
    #9
    pako69
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2020/05/06 10:50:02
    • Location: 0
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2020/05/11 13:46:59 (permalink)
    0
    gtackett
    I tried to use the 64 bit release on MacOS High Sierra (10.13), but the make that is supplied with it was linked on a later release of MacOS and doesn't work on High Sierra.
     
    A simple fix:
    1. Go to mplabx/v5.35/mplab_platform/bin
    2. [Optional, but safest] Rename or stash away a backup copy of the make that you find there.
    3. In the same folder, create a soft link, also named make, to a version of that tool that works on your system. I used gnu make which I had installed (using brew) at /usr/local/bin/gmake but you could probably just use the one at /usr/bin/make.
    Gnu make worked fine for me.


    Hi, i've the same problem on my Mac with High Sierra OS.


    Can you explain me, please step by step, all the procedure that you have made on your Mac?
    #10
    g1l1t1
    Starting Member
    • Total Posts : 23
    • Reward points : 0
    • Joined: 2020/02/27 06:19:02
    • Location: 0
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2020/05/12 09:22:43 (permalink)
    0
    $ cd /Applications/Microchip/mplabx/mplab_platform/bin
    $ mv make make_mplabx_original
    $ ln -sv /usr/bin/make make
    #11
    electricdruid
    New Member
    • Total Posts : 10
    • Reward points : 0
    • Joined: 2007/06/28 02:51:34
    • Location: 0
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2021/03/26 16:04:12 (permalink)
    0
    I'm unable to get MPLAB plus the patch to work for me.
     
    I start with a clean install of MPLAB X 5.30 and then open the makeUtilsUpdate.pkg patch, which then also installs successfully. All good so far.
    MPLAB X opens and runs but when you try and build some code, I get the following errors:
     
    sh: /Applications/microchip/mplabx/v5.30/mpasmx/mpasmx: Bad CPU type in executable
    make[2]: *** [nbproject/Makefile-default.mk:111: build/default/production/StompLFO.o] Error 1
    make[1]: *** [nbproject/Makefile-default.mk:91: .build-conf] Error 2
    make: *** [nbproject/Makefile-impl.mk:39: .build-impl] Error 2
    BUILD FAILED (exit value 2, total time: 2s)
     
    I'd use 5.45, except that the XC8 assembler isn't compatible with the asm code I've got to work with, which is a deal breaker at the moment.
     
    Any ideas what's going on gratefully appreciated.
     
    Thanks,
    Tom
    #12
    Jerry Messina
    Super Member
    • Total Posts : 715
    • Reward points : 0
    • Joined: 2003/11/07 12:35:12
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2021/03/26 16:38:40 (permalink)
    0
    While this patch allows for MPLAB X IDE to be compatible with the Catalina update, only the MPLAB XC8 compiler is currently compatible. The MPLAB XC16 and MPLAB XC32 compilers will be updated for compatibility in January

    I could be wrong, but the way I read that note the patch doesn't fix MPASM, only XC8/make. The current note says "All current versions of MPLAB XC compilers are now compatible"... no mention of MPASM, which sort of makes sense.
     
    I think you're stuck with the rest of us... 64-bit and ASM --> PIC-AS
    #13
    electricdruid
    New Member
    • Total Posts : 10
    • Reward points : 0
    • Joined: 2007/06/28 02:51:34
    • Location: 0
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2021/03/27 03:15:09 (permalink)
    0
    The work required in converting all existing code so it will assemble under PIC-AS is a considerable job that I don't need. It looks like my only option is to get OS X 10.14 Mojave installed so I can run MPLAB X 5.30 without issues.
    #14
    rjc101
    Super Member
    • Total Posts : 146
    • Reward points : 0
    • Joined: 2016/07/08 14:56:34
    • Location: 0
    • Status: offline
    Re: MAC OS Catalina 10.15 support patch 2021/03/27 05:01:52 (permalink)
    +1 (1)
    electricdruid
    The work required in converting all existing code so it will assemble under PIC-AS is a considerable job that I don't need. It looks like my only option is to get OS X 10.14 Mojave installed so I can run MPLAB X 5.30 without issues.


    Create a VM on your Mac and install the older version. I have a couple of old MacOS VM’s just to use some really old software that isn’t 64bit, and never will be.

    For some projects I keep the development environment in a VM from the start. So it can be worked on again in the future with the same tool sets as the original.
    #15
    Jump to:
    © 2021 APG vNext Commercial Version 4.5