• AVR Freaks

Hot!Class-B Safety Software

Author
Mohammed_Hassan
Starting Member
  • Total Posts : 33
  • Reward points : 0
  • Joined: 2019/03/13 06:05:20
  • Location: 0
  • Status: offline
2019/12/11 07:02:05 (permalink)
0

Class-B Safety Software

Hello Folks,
I wanna use the Class-B Safety Software to do some safety checks on my controller PIC32MZ0512EFF064.
I tried to compile the demo project which can be downloaded from microchip website but could not get it compiled! 
 
Is this library support PIC32MZ family? or only PIC32MX
 
Thanks in advance, 
#1

2 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18898
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: online
    Re: Class-B Safety Software 2019/12/11 08:32:27 (permalink)
    0
    Which Class B Library Example.
    The PIC32MZ may only be Supported in Harmony.
    #2
    Mohammed_Hassan
    Starting Member
    • Total Posts : 33
    • Reward points : 0
    • Joined: 2019/03/13 06:05:20
    • Location: 0
    • Status: offline
    Re: Class-B Safety Software 2019/12/11 08:38:03 (permalink)
    0
    NKurzman
    Which Class B Library Example.

     
     
    32-bit PIC32 ClassB Ver1.0
     
    There is a ClassB_demo.c file.
     
    NKurzman
    The PIC32MZ may only be Supported in Harmony.



    In this case Is there any way to use the library in my application? 
     
    Thanks in advance for your help as I am pretty new to PIC32 family
     
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5