• AVR Freaks

Hot!How to clean a project

Author
meeagle
Starting Member
  • Total Posts : 33
  • Reward points : 0
  • Joined: 2019/04/20 19:43:05
  • Location: 0
  • Status: offline
2019/12/10 10:09:19 (permalink)
0

How to clean a project

There is a error "fail to load the program file" after I debug to much timers, so I consider the relative files is too big, can anyone tell me how to clean a project completely? 
I use mplab x5.25, and had try "clean project" of the production menu, no effect.
#1

2 Replies Related Threads

    ric
    Super Member
    • Total Posts : 27979
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: How to clean a project 2019/12/10 13:01:01 (permalink)
    +1 (1)
    meeagle
    There is a error "fail to load the program file" after I debug to much timers,

    It would be helpful to show the entire error message.

    so I consider the relative files is too big,

    This is rubbish
     

    can anyone tell me how to clean a project completely? 
    I use mplab x5.25, and had try "clean project" of the production menu, no effect.

    What PIC chip?
    This will tell us what compiler you are using (XC32, XC16, XC8, something else???)
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    Gort2015
    Klaatu Barada Nikto
    • Total Posts : 3984
    • Reward points : 0
    • Joined: 2015/04/30 10:49:57
    • Location: 0
    • Status: offline
    Re: How to clean a project 2019/12/10 13:18:28 (permalink)
    0
    Too big !
     
    Clean project is like a fresh project compile vs compile only files that do not need ref. or change so that will not fix code bugs.

    MPLab X playing up, bug in your code? Nevermind, Star Trek:Discovery will be with us soon.
    https://www.youtube.com/watch?v=Iu1qa8N2ID0
    + ST:Continues, "What Ships are Made for", Q's back.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5