• AVR Freaks

Hot!need help solving => ICD3Err0048: Unable to set trace options

Author
art tech
Senior Member
  • Total Posts : 163
  • Reward points : 0
  • Joined: 2012/05/21 21:36:26
  • Location: 0
  • Status: offline
2019/12/08 12:40:43 (permalink)
0

need help solving => ICD3Err0048: Unable to set trace options

My code compiles fine on ICD3 with MPLAB v8.92, and programs fine, but the following error pops up and blocks all debugging functions:
 
ICD3Err0048: Unable to set trace options
 
I have JTAG disabled in the CPU config settings, so I don't think JTAG is the problem.
 
I cannot find the error "ICD3Err0048" anywhere online, so hoping someone here can offer a few suggestions of what to try.
Thanks in advance.
#1

3 Replies Related Threads

    ric
    Super Member
    • Total Posts : 25214
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: need help solving => ICD3Err0048: Unable to set trace options 2019/12/08 14:17:31 (permalink)
    0
    Is the ICD plugged directly into your PC, or via a hub?
    Is it a USB2 port, or a USB3 one?
    (USB3 ports are usually labelled "SS", or have a blue body)
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    hudejun
    Electrical engineer
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2019/12/05 08:48:06
    • Location: 0
    • Status: offline
    Re: need help solving => ICD3Err0048: Unable to set trace options 2019/12/08 15:40:29 (permalink)
    0
    - Please use latest firmware for ICD3
    - This is my experience(unscientific method)...
    I am getting various issues when use ICD3 with MPLAB X.
    JTAG option or cable connections are not problem in this case.
    At that time, I program PIC32 with project codes.
    Then, try to debug again.
     
    If still get issue, try to program and debug again.
    Of course, there are many forums with ICD3 issues.
    But, they are not solving unknown issues.
     
    #3
    art tech
    Senior Member
    • Total Posts : 163
    • Reward points : 0
    • Joined: 2012/05/21 21:36:26
    • Location: 0
    • Status: offline
    Re: need help solving => ICD3Err0048: Unable to set trace options 2019/12/08 17:27:02 (permalink)
    0
    ric
    Is the ICD plugged directly into your PC, or via a hub?
    Is it a USB2 port, or a USB3 one?
    (USB3 ports are usually labelled "SS", or have a blue body)

     
    Thanks for the quick reply. ICD3 is directly plugged to PC (no hub) on a USB 2 port. Which is better?
    I think there may be a debugger memory region conflict with a bootloader section.
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5