• AVR Freaks

Hot!Call Graph / Stack unavailable

Author
kadv
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2019/12/01 23:12:06
  • Location: 0
  • Status: offline
2019/12/02 16:16:32 (permalink)
0

Call Graph / Stack unavailable

Hello all.
 
I'm working on a PIC18C87K22 based project in MPLABX with XC8. When I right click on any function I see "Show Call Graph" in the menu but it's greyed out and unavailable. Similarly watching the call stack only shows me the most recent call - not the enrite stack as I'd expect. I have chosen a compiled stack in XC8.
 
Can anyone please offer any advice on why I can't see the graph and stack?
 
TIA.
#1

1 Reply Related Threads

    bedwards1000
    New Member
    • Total Posts : 12
    • Reward points : 0
    • Joined: 2014/05/30 14:15:14
    • Location: 0
    • Status: offline
    Re: Call Graph / Stack unavailable 2020/01/28 13:53:28 (permalink)
    +1 (1)
    I was just about to post the same question.  It was always greyed and the "Window->Call Graph" (Or "Window->Output->Call Graph" depending on which help file I was looking at) menu option didn't exist.  But I figured it out.  From the actual function I chose Navigate to Declaration/Definition and then brought up the right click menu and it worked.  From that point on it has been available on both the function and the prototype.  Go figure.
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5