• AVR Freaks

Hot!MPLAB X 5.30 hangs when trying to open a project or when creating a new project

Author
MontyBigglesworth
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2015/04/13 04:36:35
  • Location: 0
  • Status: offline
2019/11/30 09:03:41 (permalink)
0

MPLAB X 5.30 hangs when trying to open a project or when creating a new project

MPLAB X 5.3 Hangs when I create a new project.
Just after selecting the project folder location I click next and MPLAB X freezes up.
I have just found it also freezes when you select File>Open project.
Both times I have to kill MPLAB in the task manager.
I have tried installing older versions of MPLAB X (3.65 and 4.2) and the problem still exists there.
I looked online and some threads recommended the following, none of which helped.
I have tried getting the latest version of Java
I have tried disabling the firewall
 
I got so desperate I have even re-installed Windows and it didn't help!
 
I am using Windows 10 Pro 64 bit on a reasonably powerful i7 PC with 8GB of RAM so there shouldn't be any issues.
I have the XC8 compiler installed - not that I got far enough to compile anything yet!
 
The PC is pretty clean with very little installe as I just use it for lab stuff.
 
Has anyone got any suggestions?
 
FWIW I have attached a screen shot of each time it freezes.
 
In both instances this was as far as MPLAB X 3.65, 4.20 and 5.30 got before I had to kill it in task manager.

Thanks in advance!
post edited by MontyBigglesworth - 2019/11/30 09:12:46

Attachment(s)

Attachments are not available: Download requirements not met
#1

10 Replies Related Threads

    DominusT
    Super Member
    • Total Posts : 1385
    • Reward points : 0
    • Joined: 2005/07/22 08:31:18
    • Status: offline
    Re: MPLAB X 5.30 hangs when trying to open a project or when creating a new project 2019/11/30 11:51:17 (permalink)
    0
    MontyBigglesworth
    MPLAB X 5.3 Hangs when I create a new project.
    Just after selecting the project folder location I click next and MPLAB X freezes up.
    I have just found it also freezes when you select File>Open project.
    Both times I have to kill MPLAB in the task manager.
    I have tried installing older versions of MPLAB X (3.65 and 4.2) and the problem still exists there.
    I looked online and some threads recommended the following, none of which helped.
    I have tried getting the latest version of Java
    I have tried disabling the firewall
     
    I got so desperate I have even re-installed Windows and it didn't help!
     
    I am using Windows 10 Pro 64 bit on a reasonably powerful i7 PC with 8GB of RAM so there shouldn't be any issues.
    I have the XC8 compiler installed - not that I got far enough to compile anything yet!
     
    The PC is pretty clean with very little installe as I just use it for lab stuff.
     
    Has anyone got any suggestions?
     
    FWIW I have attached a screen shot of each time it freezes.
     
    In both instances this was as far as MPLAB X 3.65, 4.20 and 5.30 got before I had to kill it in task manager.

    Thanks in advance!


    I think it's something similar to what happened to me, maybe cleaning the MPLAB cache solves the problem.
     
    https://www.microchip.com/forums/FindPost/1120651
    #2
    MontyBigglesworth
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2015/04/13 04:36:35
    • Location: 0
    • Status: offline
    Re: MPLAB X 5.30 hangs when trying to open a project or when creating a new project 2019/12/05 06:02:50 (permalink)
    0
    Thanks for the suggestion. I have tried that and also tried to change the memory allocated from Java but still get freezing issues.
    It's really strange as the PC has been re-imaged from scratch and it still has the same error.
    #3
    aschen0866
    Super Member
    • Total Posts : 4544
    • Reward points : 0
    • Joined: 2006/01/08 22:18:32
    • Location: San Diego
    • Status: offline
    Re: MPLAB X 5.30 hangs when trying to open a project or when creating a new project 2019/12/05 07:41:02 (permalink)
    0
    Does this problem happen to you if you already have a project open successfully? I have formed the habit to always leave at least one project open in MPLABX before closing it.
    #4
    crennolet
    Super Member
    • Total Posts : 160
    • Reward points : 0
    • Joined: 2012/03/15 09:51:58
    • Location: 0
    • Status: offline
    Re: MPLAB X 5.30 hangs when trying to open a project or when creating a new project 2019/12/05 10:39:16 (permalink)
    0
    When you open a project in mplabx, quite a few things happen: a directory is created, and mplabx seems to try to go the network to find out if a newer version of the compiler is available, for two of these (not speaking authoritatively here, just from observation.)
     
    That suggests you might try creating the project directory in a "safe" place (on a local disk, for example, in a directory you know you have write privileges in.). And check the internet connection of the machine to make sure it's working, has the right proxy settings, etc.
     
    All just guesswork here.
    #5
    mpgmike
    Super Member
    • Total Posts : 386
    • Reward points : 0
    • Joined: 2014/01/23 17:27:06
    • Location: NJ
    • Status: offline
    Re: MPLAB X 5.30 hangs when trying to open a project or when creating a new project 2019/12/06 10:04:13 (permalink)
    +1 (1)
    I don't connect my PC to the internet (the one I use for MPLABX, not the one I'm posting on).  When it starts up, it can't find any internet connection & just skips that part.

    I don't need the world to know my name, but I want to live a life so all my great-grandchildren proudly remember me.
    #6
    Oblivion
    Starting Member
    • Total Posts : 54
    • Reward points : 0
    • Joined: 2008/10/05 00:08:00
    • Location: 0
    • Status: offline
    Re: MPLAB X 5.30 hangs when trying to open a project or when creating a new project 2019/12/08 00:59:40 (permalink)
    +1 (1)
    MPLAB X IDE v5.30 has SEVERAL issues, not just this.

    I recommend downloading an archived version and using that until MC fixes the issue(s). It's what I had to do.

    Here is a (direct, and hidden) link to the version just before V5.30
    http://ww1.microchip.com/downloads/en/DeviceDoc/MPLABX-v5.25-windows-installer.exe
    #7
    ric
    Super Member
    • Total Posts : 26038
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: MPLAB X 5.30 hangs when trying to open a project or when creating a new project 2019/12/08 01:26:06 (permalink)

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #8
    Oblivion
    Starting Member
    • Total Posts : 54
    • Reward points : 0
    • Joined: 2008/10/05 00:08:00
    • Location: 0
    • Status: offline
    Re: MPLAB X 5.30 hangs when trying to open a project or when creating a new project 2019/12/08 17:28:17 (permalink)
    0
    >The not so hidden link is:
    Except, for me, MPLAB X v5.25 isn't among the options...
    #9
    ric
    Super Member
    • Total Posts : 26038
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: MPLAB X 5.30 hangs when trying to open a project or when creating a new project 2019/12/08 17:45:14 (permalink)
    +1 (1)
    Oblivion
    >The not so hidden link is:
    Except, for me, MPLAB X v5.25 isn't among the options...

    Good point.
    Sorry for the confusion, I hadn't noticed that 5.25 isn't in the list there yet.

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #10
    tdial
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2016/08/06 09:02:04
    • Location: 0
    • Status: offline
    Re: MPLAB X 5.30 hangs when trying to open a project or when creating a new project 2020/02/17 11:17:09 (permalink)
    0
    Hello, 

    Executive summary:

         Reverting to MPLAB-X v5.10 and MCC v3.75 solved my "hangs" within the IDE, when using MCC.

    Details:
    Recently, I was struggling with MPLAB-X Version 5.30 and MCC verstion 3.95.  
     
    The behavior seemed similar to what other people are experiencing: Clicking on things within MCC caused the application to hang. Upon inspection in "top", I noticed that the application was using approx 53% CPU. I previosuly suspected conflicts with JVM versions on my machine until I realized that MPLABX shipped with its own JRE.

    I ruled out all hardware issues on my computer. Likewise, I was able to reproduce the issue on two configurations of computers:
    * HP Z820 Running Debian 10.3 Linux (2x8 core Xeon, 64 GB RAM)
    * Macbook Pro 2016 i7 (16 GB RAM) Running Mojave

    After struggling with this for hours and attempting to find a solution, I've arrived at a previous version of MPLAB-X and MCC that work for me:

    * MPLABX - Version 5.10 (Archive Page: Choose your platform)
    https://www.microchip.com/development-tools/pic-and-dspic-downloads-archive
    * MCC - Version 3.75 (Direct Link)
    http://www.microchip.com/mymicrochip/filehandler.aspx?ddocname=en609631

    My procedure for installing was as follows - naturally, follow at your own risk!

    1. **IMPORTANT** -  As always - make a backup of any projects or directories that may contain valuable data.
    2. Uninstall any verion(s) of MPLAB that exist (this may not be strictly necessary, but I wanted to start clean.)
    3. Install MPLABX v5.10
    4. Unzip MCC Plugin downloaded above to extract the *.nbm file
    5. Start MPLABX.  From the Tools Menu, select "Plugins" to launch the plugin dialog.  Choose the Downloaded tab.
    6. Click Add Plugins.. button and the browse to the path to version 3.75 of the MCC nbm.
    7. Install the plugin

    My experiments with other MPLABX / MCC failed for various reasons.  One previous version, I believe 5.20, forced me to update MCC to 3.95. Version 5.10 of MPLABX did NOT force me to update, although it constantly nags you to do so.  I sort of assume that what's causing everyone problem is the later plugin version of MCC (v3.95).

    DISCLAIMER: I'm just a hobbyist with no affiliation to Microchip, so any statements I'm making are obviously speculation.  Please proceed at your own risk. If anyone from Microchip is reading this comment, I would gladly upgrade to what appears to be the troublesome 5.30 version to help you gather data about what's going on. I am a fairly experienced (e.g. 20 years) professional software guy with deep experience debugging Linux applications and also have Java experience.  I believe the issue is with v3.95 of the MCC plugin because I have an issue with it on both platforms that I've tested.
     
     
    #11
    Jump to:
    © 2020 APG vNext Commercial Version 4.5