• AVR Freaks

Hot!Getting started with AC164159

Author
Human
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/03/27 00:03:39
  • Location: 0
  • Status: offline
2019/11/26 00:32:28 (permalink)
5 (1)

Getting started with AC164159

Hello, I have purchased AC164159 that has SAMR30M18A module. I have read the product page and I would appreciate if anyone provides me a summary of how I can start developing the application.
1: I have installed atmel studio, need to know the for RF communication, miwi is mandatory or recommended.
2: Which libraries are there for developing RF applications for SAMR30M18A module.
3: I also have 10 SAMR30M18A modules, do I need to have a programmer for loading the firmware or can it be done using this kit AC164159?
 
I appreciate your feedback.
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5