• AVR Freaks

Hot!Configuration bits "Generator Source code“ to output disabled

Author
ah1008
New Member
  • Total Posts : 22
  • Reward points : 0
  • Joined: 2019/11/20 00:08:45
  • Location: China
  • Status: offline
2019/11/20 19:03:39 (permalink)
0

Configuration bits "Generator Source code“ to output disabled

Hi experts.
          I am working on ATSAME53N20A  with arm tool chain in MPLAB X v5.30.
          One question: when I read the configration bits , how can I use the Generator Souce code button ".
           That one is disabled .???
 
Thanks,
Alex

Attachment(s)

Attachments are not available: Download requirements not met
#1

3 Replies Related Threads

    saulo96
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2019/09/23 09:04:51
    • Location: 0
    • Status: offline
    Re: Configuration bits "Generator Source code“ to output disabled 2020/07/05 19:04:07 (permalink)
    0
    Hi,
     
    I'm having the exact same issue with PICF18258, it is my first project and Im trying to get this info from the manual, but I really couldn't find it.
     
    Did you managed to solve the problem?
     
    Saulo.
    #2
    ric
    Super Member
    • Total Posts : 28009
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Configuration bits "Generator Source code“ to output disabled 2020/07/05 19:32:08 (permalink)
    0
    saulo96
    I'm having the exact same issue with PICF18258, it is my first project and Im trying to get this info from the manual, but I really couldn't find it.

    Which compiler/assembler have you selected for your project?
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #3
    ah1008
    New Member
    • Total Posts : 22
    • Reward points : 0
    • Joined: 2019/11/20 00:08:45
    • Location: China
    • Status: offline
    Re: Configuration bits "Generator Source code“ to output disabled 2020/07/05 23:00:11 (permalink)
    0
    Yes. In my case , I try to use arm gcc to parse the Macros are only supported by XC32.
     
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5