• AVR Freaks

Helpful ReplyHot!is there some way to set the Radix setting for a XC8 LST file?

Author
bxdobs
Junior Member
  • Total Posts : 42
  • Reward points : 0
  • Joined: 2014/10/13 18:05:44
  • Location: 0
  • Status: offline
2019/11/20 15:28:19 (permalink)
5 (1)

is there some way to set the Radix setting for a XC8 LST file?

in assembler mode there is the option to set things like: r=hex and p=16F88
in the XC8 Manual there is discussion of: OPT LIST r=hex
but I'm not following where this can be used
if put in the header of a c file the compiler complains about OPT not being defined
if enclosed in asm(""); similar error
if added to the Make options the MAKE fails
 
Does anyone know how this was meant to be implemented?
Looking to have the ASM listing (lst file) is in HEX instead of DECIMAL
 
#1
mad_c
Super Member
  • Total Posts : 1245
  • Reward points : 0
  • Joined: 2010/12/12 17:48:27
  • Location: Brisbane, Australia
  • Status: offline
Re: is there some way to set the Radix setting for a XC8 LST file? 2019/11/21 13:44:43 (permalink) ☄ Helpfulby Jim Nickerson 2019/11/22 07:56:10
+1 (1)
bxdobs
in assembler mode there is the option to set things like: r=hex and p=16F88
in the XC8 Manual there is discussion of: OPT LIST r=hex
but I'm not following where this can be used
 

Hi,
 
Assembler controls are meant to be placed in assembly code; however, after looking at the assembler source, the LIST control is still present, but all the options for it have been disabled. I'll need to check whether that was intentionally done to prevent some issue, or if they accidentally 'fell off'. I can't see any other way to control the listing radix.
 
Jeff.
#2
Jump to:
© 2020 APG vNext Commercial Version 4.5