• AVR Freaks

Hot!What code is the Curiosity HPC (DM164136) shipped with?

Author
dwegscheid
New Member
  • Total Posts : 12
  • Reward points : 0
  • Joined: 2019/07/25 05:20:53
  • Location: 0
  • Status: offline
2019/11/19 13:53:25 (permalink)
0

What code is the Curiosity HPC (DM164136) shipped with?

I just unboxed my DM164136, and was pleasantly surprised to see it was running some code.
 
Apparently it lights D5 if S1 is depressed, lights D4 if S2 is depressed, and varies the brightness of D3 depending on the position of the pot.
 
Where is the source code for this? It does not seem to be in the "Curiosity HPC Demo Code" shown on https://www.microchip.com...oductDetails/DM164136.
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5