• AVR Freaks

Hot!MPLAB X (XC16) not tracking struct defines properly

Author
JimWoodworker
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2018/10/25 13:40:41
  • Location: 0
  • Status: offline
2019/11/18 10:46:39 (permalink)
0

MPLAB X (XC16) not tracking struct defines properly

I recently began having issues with MPLAB X IDE (and it might be an issue related to MPLAB XC16) not tracking variables that are part of a defined struct properly and highlighting.  The project compiles correctly. 
 
The code areas that have problems look something like this (also attached a snip of the editor window to this message):
kbus_rsData.item.instRPM = 0;
kbus_rsData.item.avgRPM = 0;
kbus_rsData.item.toolface = 0xffff;
kbus_rsData.item.defl = 0x7f;
 
It highlights at the .item level of the struct definition.
 
I also can no longer right click on item or elements under item and select navigate\go to declaration/definition anymore either.
 
This worked at one time.  What IDE or XC16 settings do I need to go into to fix this and get the IDE to regenerate the variables table so it knows where all the definitions are located?
 
 

Attachment(s)

Attachments are not available: Download requirements not met
#1

2 Replies Related Threads

    domble
    Senior Member
    • Total Posts : 136
    • Reward points : 0
    • Joined: 2007/01/25 04:11:53
    • Location: 0
    • Status: offline
    Re: MPLAB X (XC16) not tracking struct defines properly 2019/11/19 10:01:31 (permalink)
    +1 (1)
    Compile the code might help, or the usual right click in on top of project tree, select "code assistance" then "reparse project".
     
    dom.
    #2
    JimWoodworker
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2018/10/25 13:40:41
    • Location: 0
    • Status: offline
    Re: MPLAB X (XC16) not tracking struct defines properly 2019/11/19 10:09:02 (permalink)
    0
    Thanks for you suggestion.
     
    Compiling code didn't do anything and I had done that plenty before posting my question to the forum.
     
    However right clicking on the project and selecting code assistance\reparse project worked like a charm.
     
    Thank You!!
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5