• AVR Freaks

Hot!Building Bm7x_configure_demo.X for RN4870

Author
davidif
Senior Member
  • Total Posts : 127
  • Reward points : 0
  • Joined: 2013/11/16 05:47:28
  • Location: 0
  • Status: offline
2019/11/15 10:37:19 (permalink)
0

Building Bm7x_configure_demo.X for RN4870

Hello,
I start programming the RN4870 module on the starter kit and I would like to use it with a pic32mx795F512l.
I am oriented on the program example "bm7x_configure_demo.X" or started I can not compile it, plib.h is not found?
I tried with different version of the XC32 compiler but without success
 
make[2]: *** [build/PIC32/production/_ext/812168374/uart_drv.o] Error 1
make[2]: *** Waiting for unfinished jobs....
make[2]: *** [build/PIC32/production/_ext/812168374/time.o] Error 1
make[2]: *** [build/PIC32/production/_ext/812168374/uart_app.o] Error 1
In file included from ../source/main.c:72:0:
../source/time.h:38:21: fatal error: plib.h: No such file or directory
#include "plib.h"
 
i use mplab IDE V5.25
XC2.30 et below too
 
Perhaps there is another more appropriate example ...
I also watched the one under harmony:
C: \ microchip \ harmony \ v2_06 \ apps \ bluetooth \ data \ ble_rn4871_comm \ firmware \ ble_rn4871_comm.X but I get the impression that it does not use the RN4870 module, I do not see an init file. .. or maybe I have to do it myself? ...
 
Thank for your help 
#1

1 Reply Related Threads

    Jim Nickerson
    User 452
    • Total Posts : 6688
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: online
    Jump to:
    © 2020 APG vNext Commercial Version 4.5