• AVR Freaks

Hot!Harmony v2.06 USB not working PIC32MZ2048EFH064

Page: < 12 Showing page 2 of 2
Author
NKurzman
A Guy on the Net
  • Total Posts : 19043
  • Reward points : 0
  • Joined: 2008/01/16 19:33:48
  • Location: 0
  • Status: offline
Re: Harmony v2.06 USB not working PIC32MZ2048EFH064 2019/12/18 09:56:11 (permalink)
0
lelsteph
Hello
 
Master ? Slave? I do not recognize this terminology in the USB world. The PIC is a USB Powered Device (see configuration in initial post).
 
If you add a too big capacitor, I do not think this is good.
 
Stephane.
 


The USB Terminology is "Host" and "Device".  Your Project is a CDC Device according to your First post.?
#21
Howard Long
Super Member
  • Total Posts : 845
  • Reward points : 0
  • Joined: 2005/04/04 08:50:32
  • Status: offline
Re: Harmony v2.06 USB not working PIC32MZ2048EFH064 2019/12/18 10:10:47 (permalink)
0
lelsteph
 
Master ? Slave? I do not recognize this terminology in the USB world. The PIC is a USB Powered Device (see configuration in initial post).
 
If you add a too big capacitor, I do not think this is good.

 
I agree, for a USB device ISTR the maximum is 10uF Vbus capacitance.
 
#22
lelsteph
Super Member
  • Total Posts : 405
  • Reward points : 0
  • Joined: 2008/09/17 05:10:00
  • Location: 0
  • Status: offline
Re: Harmony v2.06 USB not working PIC32MZ2048EFH064 2019/12/18 11:35:47 (permalink)
0
Hello
 
@NKurzman: Yes USB CDC Device, we are aligned on the terminology
 
@Howard: ;)
 
Stephane.
#23
Page: < 12 Showing page 2 of 2
Jump to:
© 2020 APG vNext Commercial Version 4.5