• AVR Freaks

Hot!advisory: (2051) The current license does not permit optimization level" after HPA update

Author
spash
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/09/25 01:55:21
  • Location: 0
  • Status: offline
2019/11/12 07:00:15 (permalink)
5 (1)

advisory: (2051) The current license does not permit optimization level" after HPA update

Hi,
We have a SW006021-VM MPLAB XC Virtual Machine License for Pro Network Server Compilers and a SW006021-2N MPLAB XC8 PRO Compiler (Network Server License).
We renewed the HPA for the XC8 compiler, downloaded and redeployed the VM and Compiler licences on the RLM server.
If we use a XC 8 compiler 2.1, we have an "advisory: (2051) The current license does not permit the selected optimization level, using optimization level 2".
If we use a XC8 1.x compiler, licence is in PRO mode as expected.
xclm -licinfo xc8 returns:

"C:\Program Files (x86)\Microchip\xc8\v2.10\bin\xclm" -licinfo xc8
Type=Network
Version=1.0
Mode=PRO
Key=<key of the licence>
Seats=3
Available=2

 
Could you please explain/help on what is wrong ?
Isn't the HPA valid for all major versions of the compiler ? What should we do to be able to use the 2.10 pro features ?
Thank you.
#1

2 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18798
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: advisory: (2051) The current license does not permit optimization level" after HPA upd 2019/11/12 08:47:03 (permalink)
    +2 (2)
    If your HPA is not expired.
    Contact swLicensing@ Microchip.com
    #2
    spash
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2019/09/25 01:55:21
    • Location: 0
    • Status: offline
    Re: advisory: (2051) The current license does not permit optimization level" after HPA upd 2019/11/13 02:13:42 (permalink)
    +2 (2)
    For those who might find it useful, got working solution from swlicensing email support: remove old licences from RLM, deploy new ones, and restart RLM server.
     
     
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5