• AVR Freaks

Hot!ICD3 can't read and write whole PIC memory

Author
Kabak
Starting Member
  • Total Posts : 87
  • Reward points : 0
  • Joined: 2014/07/30 03:47:55
  • Location: 0
  • Status: offline
2019/11/12 05:21:38 (permalink)
0

ICD3 can't read and write whole PIC memory

Hi
My ICD3 10-00421-R3 SN: JIT140211527 work with testing board and visible to MPLAB8 / MPLABX under Windows 10 x64 , switching between them using MPDDSwitch64.exe , has latest firmware, but it read and write into PIC18F2620 till 0800x address. No onchip EEPROM reading or writing occurred.

Could you be so kind to help me with that problem ?

Than you.
 
post edited by Kabak - 2019/11/12 05:34:40
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5