• AVR Freaks

Hot!Trying to program PIC10F200

Author
tmostad
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/11/04 15:21:45
  • Location: 0
  • Status: offline
2019/11/08 17:53:14 (permalink)
0

Trying to program PIC10F200

I am trying to program a PIC10F200 with an ICD4. It will connect and erase the device but then fails to verify:
 
Verify failed.  [ Pgm ] at 0x3, expected 0x00000c0b, got 0x00000402
Programming did not complete.
 
Any ideas?
#1

4 Replies Related Threads

    ric
    Super Member
    • Total Posts : 25125
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Trying to program PIC10F200 2019/11/08 23:41:19 (permalink)
    5 (1)
    There is no "device ID" word in PIC10F20x chips, so the programmer has no idea if it is really "connected" to the device correctly.
    (That's yet another reason why it's a good idea to upgrade to PIC10F322)
    How exactly do you physically have the PIC connected to the ICD4?
    What is powering the PIC?
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    newfound
    Super Member
    • Total Posts : 1849
    • Reward points : 0
    • Joined: 2003/11/07 12:35:49
    • Status: offline
    Re: Trying to program PIC10F200 2019/11/09 01:13:40 (permalink)
    0
    The device appears to not be erased properly. The minimum erase Vdd voltage for this part is 4.5V
    #3
    tmostad
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2019/11/04 15:21:45
    • Location: 0
    • Status: offline
    Re: Trying to program PIC10F200 2019/11/09 07:39:14 (permalink)
    0
    I missed that there is a separate programming specification and yes it says that 5V Vdd is needed. I am going to switch to the 320 since it can be programmed at vddmin which can be far less than 3.3V.
     
    BTW - My physical connection to the board is through a Tag-Connect cable which seems to work very nicely.
    #4
    tmostad
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2019/11/04 15:21:45
    • Location: 0
    • Status: offline
    Re: Trying to program PIC10F200 2019/11/12 14:51:33 (permalink)
    4 (2)
    Got the PIC10F320's and replaced the 200. Everything programs perfectly and my app is running great. Thanks for the help!
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5