• AVR Freaks

Hot!Refuses to enter ICSP / debug mode on PIC24FJ64GA702

Author
user2x
Super Member
  • Total Posts : 352
  • Reward points : 0
  • Joined: 2011/02/10 20:43:36
  • Location: 0
  • Status: offline
2019/11/07 17:43:34 (permalink)
0

Refuses to enter ICSP / debug mode on PIC24FJ64GA702

Panic.
 
I just received 50 boards ready to go but they refuse to be programmed. (I tried 4 of them)
 
I checked the voltage levels and they are ok, including the 1.8V on pin VCAP.
 
This worked on my prototype and the only difference of note is that I have a 4k7 pullup on the MCLR instead of the 10k as previous.
 
I checked the waveform on MCLR and it is a high pulse of 496us and nthen drops down to 0 and reaches that at 522us.
That is a tiny bit more than the P21 in the spec sheet stating 500us max.
 
Would that be the reason that it does not work?
 
If not, what else should I check?
 
This spec:
PIC24FJ256GA705 FamilyFlash Programming Specification
 
 
The message from MPLAB is :
"The Device ID (0xffff0000) is an invalid Device ID. Please check your connections...."
 
 
 
#1

4 Replies Related Threads

    ric
    Super Member
    • Total Posts : 25116
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Refuses to enter ICSP / debug mode on PIC24FJ64GA702 2019/11/07 17:46:28 (permalink)
    0
    Did you try changing the pullup back to 10k?
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    user2x
    Super Member
    • Total Posts : 352
    • Reward points : 0
    • Joined: 2011/02/10 20:43:36
    • Location: 0
    • Status: offline
    Re: Refuses to enter ICSP / debug mode on PIC24FJ64GA702 2019/11/07 17:55:16 (permalink)
    5 (1)
    Crisis averted!!
     
    The problem was that MPLAB 5.10 had crashed in some subtle non evident way.
     
    Perhaps it was because I used the IPE in between. I am not sure but for whatever reason, MPLAB was the problem.
     
    Once I restarted the lot, it suddenly started loading firmware into the ICD3 and then everything worked again.
     
    Oh man, what a start to a Friday.
     
    X
    #3
    maxruben
    Super Member
    • Total Posts : 3373
    • Reward points : 0
    • Joined: 2011/02/22 03:35:11
    • Location: Sweden
    • Status: offline
    Re: Refuses to enter ICSP / debug mode on PIC24FJ64GA702 2019/11/08 02:59:07 (permalink)
    0
    Good you found the reason before end of Friday. Otherwise the weekend would have been ruined Smile: Smile
     
    /Ruben
    #4
    NorthGuy
    Super Member
    • Total Posts : 5868
    • Reward points : 0
    • Joined: 2014/02/23 14:23:23
    • Location: Northern Canada
    • Status: offline
    Re: Refuses to enter ICSP / debug mode on PIC24FJ64GA702 2019/11/08 08:13:13 (permalink)
    5 (1)
    If you printed 10,000 boards, the whole experience would be much more interesting :)
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5