• AVR Freaks

Hot!V3 MH Configurator Export - Exporter list is empty - Is Yours

Author
jkelleher
Starting Member
  • Total Posts : 16
  • Reward points : 0
  • Joined: 2014/11/21 10:02:11
  • Location: 0
  • Status: offline
2019/10/29 06:50:24 (permalink)
0

V3 MH Configurator Export - Exporter list is empty - Is Yours

Hi I'm new to Harmony and I'm starting with Version 3 (no V2 experience - so a I'm a newbie).  I'm working on a new project for the bootloader.  I'm trying to figure out how to load the pin configurations for a 144 pin device, without manually entering each one again.  Web searches bring up V2 using the MHC's Export menu command. 
 
When in V3 MHC, the popup export menu doesn't bring up any options, do I need to download a plugin or something?  Or is this another V3 coming soon....,  OR is there another way to bring my pins from one project to a new bootloader project I'm creating?
 
My Project is for a PIC32MZ2048EFG144, and I'm using all the latest on Mac OSx mplabx and harmony 3(git pull)

 
Thanks,
Jim
 
post edited by jkelleher - 2019/10/29 06:56:29

Attached Image(s)

#1

6 Replies Related Threads

    EngSam
    New Member
    • Total Posts : 19
    • Reward points : 0
    • Joined: 2019/04/17 09:28:54
    • Location: 0
    • Status: offline
    Re: V3 MH Configurator Export - Exporter list is empty - Is Yours 2020/04/07 06:59:09 (permalink)
    0
    same here :(
    no exporter PIC32mk
    #2
    Vincent44
    Starting Member
    • Total Posts : 52
    • Reward points : 0
    • Joined: 2014/09/19 03:41:47
    • Location: France
    • Status: offline
    Re: V3 MH Configurator Export - Exporter list is empty - Is Yours 2020/05/22 03:57:51 (permalink)
    0
    Did you get any news on that matter ?
    I am facing the exact same issue : trying to import/export some parameters that I need to share between my app and bootloader, but the export menu is empty. From what I understand, you could manually copy/paste the related line in the configuration xml file, but it's not a very clean solution ...
    #3
    mpamplona
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2020/05/28 03:55:26
    • Location: 0
    • Status: offline
    Re: V3 MH Configurator Export - Exporter list is empty - Is Yours 2020/06/01 05:12:35 (permalink)
    0
    Same here !
    #4
    RISC
    Super Member
    • Total Posts : 5788
    • Reward points : 0
    • Status: online
    Re: V3 MH Configurator Export - Exporter list is empty - Is Yours 2020/06/02 02:47:40 (permalink)
    0
    Hi,
    I believe this is related to the same issue I had with Harmony content manager back in march 2020.
    I thought that this had been published in Harmony repos in the meantime.
    I got the following file from Microchip technical support (Windows version) to replace the existing harmony-content-manager.JAR file 
    Locate this file in your Harmony installation and just replace it. It solved the issue for me.
    Remove the .txt at the end it is a zip file
    Regards
    #5
    Vincent44
    Starting Member
    • Total Posts : 52
    • Reward points : 0
    • Joined: 2014/09/19 03:41:47
    • Location: France
    • Status: offline
    Re: V3 MH Configurator Export - Exporter list is empty - Is Yours 2020/06/02 02:50:34 (permalink)
    0
    Thanks RISC, I'll look into this.
    Manually changing the file is a bit annoying, especially when you need to ensure all your team is doing it...
     
    In the meantime, I opened a support ticket to get an "official" info. Hopefully, this issue will be solved in the next release of Harmony.
    #6
    Vincent44
    Starting Member
    • Total Posts : 52
    • Reward points : 0
    • Joined: 2014/09/19 03:41:47
    • Location: France
    • Status: offline
    Re: V3 MH Configurator Export - Exporter list is empty - Is Yours 2020/06/02 03:32:27 (permalink)
    0
    Just receive the answer to my support ticket.
     
    Microchip support
    There are some features in the Harmony3 Plugin that is not yet fully implemented, and one of them is the block import/ export feature. There is no official timeline yet on when will this be implemented.
    There is one option you can try which is the IDE > MHC > 'Save State As' and 'Load State', although this will save and load the whole Project Graph, which I think is not the feature you are looking for.
    So for now, users will have to manually copy the Configuration Options from one project to another.
    Personally, when I copy an existing configuration, I open 2 instances of MPLABX IDE then position them side-by-side so I can easily compare the two. If you are not aware of it yet, you can setup multiple IDE instances following this Developer Help guide:
    https://microchipdeveloper.com/mplabx:instances



    No the answer I was expecting, but at least we now have the confirmation that his feature is not working.
    #7
    Jump to:
    © 2020 APG vNext Commercial Version 4.5