• AVR Freaks

dsPIC33CK256MP508 DMA peripheral to peripheral transfer HELP

Author
mjphillips1
New Member
  • Total Posts : 26
  • Reward points : 0
  • Joined: 2009/10/21 12:27:11
  • Location: Youngstown, Ohio
  • Status: offline
2019/10/28 06:37:58 (permalink)
0

dsPIC33CK256MP508 DMA peripheral to peripheral transfer HELP

Hello all,
 
I am hoping someone could point me in the right direction on an example or guidence with using the DMA to transfer between two UART modules of the dspic33CK series.  I have already tried to use the examples in the dspic references but the DMA module for the CK series is slightly different and I am unsure what to modify.  
 
Currently I am trying to use the curiosity board with a RN4871 click attached.  I want to use the onboard USB-UART to pass messages to and from teraterm to the RN4871.  I have the RN4871 setup to use UART2.  So whenever I receive characters from teraterm I want to pass them along to the RN4871 and when I receive characters from the RN4871 I want to display them on teraterm.  
 
I am going to set up the RN4871 up as transparent UART.  
 
Any help would be appreciated.
 
Thanks,
Mike

Mike Phillips
Electrical Engineer
https://play.google.com/s....pictimercalculatorpro
 
#1

0 Replies Related Threads

    Jump to:
    © 2021 APG vNext Commercial Version 4.5