• AVR Freaks

Hot!Harmony v3 with LCC

Author
darren
Starting Member
  • Total Posts : 64
  • Reward points : 0
  • Joined: 2010/10/02 04:31:04
  • Location: 0
  • Status: offline
2019/10/21 06:38:29 (permalink)
0

Harmony v3 with LCC

Hi,
 
I'm exploring the idea of using a PIC32MX with LCC for a graphics project. I'm trying to around harmony v3, creating new projects etc... but when I try to include the LCC an error comes up:
 
<Configuration Database>[Error]: Failed to activate component: gfx_driver_lcc
 
Any idea about this error? Does harmony v3 support LCC or should I just use v2?
 
Thanks
#1

2 Replies Related Threads

    MHGC
    Super Member
    • Total Posts : 245
    • Reward points : 0
    • Status: offline
    Re: Harmony v3 with LCC 2019/10/21 08:50:00 (permalink)
    0
    Hi,
     
    Graphics for PIC32MX is currently not support with Harmony v3.  There are plans to add support back in a future Harmony 3 release.
     
    However, there are other development kit of similar capability that is supported in Harmony v3.
    Such as this:
    https://www.microchip.com/Developmenttools/ProductDetails/DM320210
    or
    https://www.microchip.com/Developmenttools/ProductDetails/DM320113
     
    PIC32MZ EF is also supported in Harmony v3.
     
    #2
    darren
    Starting Member
    • Total Posts : 64
    • Reward points : 0
    • Joined: 2010/10/02 04:31:04
    • Location: 0
    • Status: offline
    Re: Harmony v3 with LCC 2019/10/22 00:59:14 (permalink)
    0
    Hi,
     
    Thanks for your reply. I created a project using both the SAME54 and SAME70 and tried to use the MPLAB Harmony 3 Configurator. When I try to select the LCC, it gives me again the same error. Is LCC supported in Harmony v3? 
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5