• AVR Freaks

Hot!MCP39F511 bit4 status

Author
LECAT
Senior Member
  • Total Posts : 121
  • Reward points : 0
  • Joined: 2012/01/24 03:23:44
  • Location: MONTPELLIER FRANCE
  • Status: offline
2019/10/19 00:54:47 (permalink)
0

MCP39F511 bit4 status

Good morning all.
I use the MCP39f511, it works well but I have a small problem with the bit4 of the STATUS, this bit bit gives the sign of the active power. my problem !!! when the power is in one direction the byte of low weight = 0x01 it is ok but when the power reverses the low weight passes to 0x11 only from -300W which corresponds to a tension between I + and I- 60mV (for the MCP)
can I set the switch to 0x11 closer to 0W?
I hope I was clear in my explanation
thank you
Franck
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5