• AVR Freaks

MPLAB SNAP wiring harness for PIC32MZ EF SK - J7 ICSP - smaller .050" header

Author
sl149q
New Member
  • Total Posts : 9
  • Reward points : 0
  • Joined: 2013/09/24 15:42:30
  • Location: 0
  • Status: offline
2019/10/18 15:21:46 (permalink)
0

MPLAB SNAP wiring harness for PIC32MZ EF SK - J7 ICSP - smaller .050" header

What wiring harness do I need to use the MPLAB SNAP programmer with the PIC32MZ EF Starter Kit?
The J7 ICSP header has a smaller pitch than the SNAP connector or the TPROG001 wiring harness.
The PIC32MZ EF SK User's Guide says that the header is:
     J7 CONN HEADER .050" 6POS PCB GOLD

Thanks!
#1

1 Reply Related Threads

    sl149q
    New Member
    • Total Posts : 9
    • Reward points : 0
    • Joined: 2013/09/24 15:42:30
    • Location: 0
    • Status: offline
    Re: MPLAB SNAP wiring harness for PIC32MZ EF SK - J7 ICSP - smaller .050" header 2019/10/24 11:14:52 (permalink)
    0
    This adapter board from Olimex is not a perfect fit for the PIC32MZ EF SK small ICSP header but does work.

    https://www.digikey.ca/pr...20LTD%20%2F%20PIC-ICSP
    #2
    Jump to:
    © 2021 APG vNext Commercial Version 4.5