• AVR Freaks

Hot!MCC Pin Manager has wrong pinout for ATtiny412 (?)

Author
jventerprises
New Member
  • Total Posts : 25
  • Reward points : 0
  • Joined: 2011/10/13 18:01:46
  • Location: 0
  • Status: offline
2019/10/17 16:14:09 (permalink)
0

MCC Pin Manager has wrong pinout for ATtiny412 (?)

I must be missing something, but when i look at the pinout for the ATtiny412 in the MCC Pin manager I see image 1, and the datasheet shows image 2.
 
Am i nuts?  looks like PA2 and PA1 are swapped.
 
If I am not nuts, can i fix that somehow?
 
 
 
 
 

Attached Image(s)

#1

4 Replies Related Threads

    du00000001
    Just Some Member
    • Total Posts : 3777
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: online
    Re: MCC Pin Manager has wrong pinout for ATtiny412 (?) 2019/10/17 17:29:12 (permalink)
    0

    ... can I fix that somehow?

    Provided you are able to locate the image file MCC is using ... (I assume it's just some static graphics), you could modify this file. (If it's generated from some .xml: you can modify this as well.)
     
    For normal applications, the wrong image may be considered a nuissance. But it has no effect on the device configuration. So I personally wouldn't invest the effort to correct that.
    But it would make sense to notify MCC support about this issue...

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #2
    ric
    Super Member
    • Total Posts : 27624
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: MCC Pin Manager has wrong pinout for ATtiny412 (?) 2019/10/17 17:36:02 (permalink)
    0
    du00000001
    But it would make sense to notify MCC support about this issue...

    and the official way to do that is via a "Support Ticket". http://microchip.com/support
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #3
    jventerprises
    New Member
    • Total Posts : 25
    • Reward points : 0
    • Joined: 2011/10/13 18:01:46
    • Location: 0
    • Status: offline
    Re: MCC Pin Manager has wrong pinout for ATtiny412 (?) 2019/10/17 17:47:14 (permalink)
    0
    Will do, thanks.
     
     
    #4
    je_ruud
    Starting Member
    • Total Posts : 11
    • Reward points : 0
    • Joined: 2016/12/08 23:55:38
    • Location: 0
    • Status: offline
    Re: MCC Pin Manager has wrong pinout for ATtiny412 (?) 2019/10/18 00:58:03 (permalink)
    0
    Yes, they are swapped, and it will be fixed in the next update of the ATtiny_DFP.
     
    The issue is present on ATtiny202/212/402/412.
    #5
    Jump to:
    © 2020 APG vNext Commercial Version 4.5