• AVR Freaks

Hot!Want to get the layout of the DM320007

Author
KevinHuang
New Member
  • Total Posts : 23
  • Reward points : 0
  • Joined: 2019/08/29 08:13:33
  • Location: 0
  • Status: offline
2019/10/17 15:44:44 (permalink)
0

Want to get the layout of the DM320007

Hi,
 
I'm looking for the layout of the DM320007.
 
Currently I'm fighting with a project to push SPI data to Ethernet.
With DM320007, everything looks fine. Same code with myself PCB (with only the same pic32 and the same Ethernet chip), I constantly read SPI data with wrong sequence.
At the beginning I thought may be the PKOB on the DM320007 helps to correct the data sequence. However I removed all unrelated chips from the DM320007, the DM320007 still works fine with the same code. So I'm worrying about my layout.
https://www.microchip.com/forums/m1115705.aspx
 
On Microchip's website of the DM320007, it only has the user manual with schematic. 
 
Could anyone tell me, where I can get the DM320007's PCB layout file? I appreciate your help.
 
Bests,
--- Kevin
 
#1

1 Reply Related Threads

    KevinHuang
    New Member
    • Total Posts : 23
    • Reward points : 0
    • Joined: 2019/08/29 08:13:33
    • Location: 0
    • Status: offline
    Re: Want to get the layout of the DM320007 2019/10/18 14:52:32 (permalink)
    4 (1)
    Problem solved. The wires on the DM320007 have Parasitic capacitance, but my PCB doesn't. 47pF capacitor added, and now problem solved.
    Thanks for your reading.
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5