• AVR Freaks

Hot!SPI5 & Sensors

Author
seacher
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/10/15 06:07:49
  • Location: 0
  • Status: offline
2019/10/17 00:14:41 (permalink)
0

SPI5 & Sensors

Hello Guys,
i am Student. i have to work of a project with SPI5-protocol and Sensors.
my task consist to contruct an ECU, which establish a communication between Uc and Sensors.
this communication schould use the SPI5 Protocol.
I don't have big experiance with Electronic.
please i want to have some advice:
- how can i start it? how can i implemate the spi5 protcol in the uC??
- how can i add sensors to triger a communication between them?
 
thanks a lot
#1

1 Reply Related Threads

    ric
    Super Member
    • Total Posts : 27057
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: SPI5 & Sensors 2019/10/17 12:36:03 (permalink)
    +1 (1)
    What is your experience? Have you programmed ANY microcontroller before?
    Do you intend working in C, or machine language?
    Have you selected a PIC device to use?
    Do you have a working PCB with one of these PIC devices on it? (e.g. a Microchip evaluation board?)
    Do you have enough knowledge to get this board to flash an LED once per second?
    Do you have documentation for this "SPI5" protocol?
    (The only match I found with a quick Google search is "The SPI-5 draft standard is the fifth-generation definition of the SCSI-3 Physical Layer.")
     
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5