• AVR Freaks

Hot!MDD_ROOT_DIR_PATH

Author
uomotigre
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/05/30 11:25:03
  • Location: 0
  • Status: offline
2019/10/14 11:12:38 (permalink)
0

MDD_ROOT_DIR_PATH

somebody can help about this issue below:

I tried to configurate my tcpip stack with an sd-card. when I launching my ip address the page open but not fully. Probabily the root directory is not properly configurated, but i am not sure.

The original root path (TCPIPConfig.h) from microchip  is '#define MDD_ROOT_DIR_PATH   "\\WWW\\" '  but this define doesn't work! So I changed to  #define MDD_ROOT_DIR_PATH  "\\"  now I can open my page but of course is incorrectly. I suspect the page open without the .css file and header.inc. I think problems are with directory that are not properly configurate, really I cannot understanding. Below the photo that I recived from sd card.
 
in advance too much appreciate if somebody help me

Attached Image(s)

#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5