• AVR Freaks

Hot!Harmony v3 USART Read/Write Bytes

Author
ryanjones
New Member
  • Total Posts : 9
  • Reward points : 0
  • Joined: 2019/01/07 13:51:21
  • Location: 0
  • Status: offline
2019/10/13 19:58:25 (permalink)
0

Harmony v3 USART Read/Write Bytes

Currently trying to move a project to a new chip and having to change from harmony v2.06 to harmony v3, and having some problems around the USART drivers.
The old system used the static DRV_USARTx drivers to read and write bytes individually. Is there a way to replicate these functions in Harmony V3 easily or will I have to use the DRV_USART_WriteBufferAdd functions and pass in the DRV_HANDLE and DRV_USART_BUFFER_HANDLE?
 
Thanks
#1

1 Reply Related Threads

    lcitos
    New Member
    • Total Posts : 10
    • Reward points : 0
    • Joined: 2019/07/01 10:58:01
    • Location: 0
    • Status: offline
    Re: Harmony v3 USART Read/Write Bytes 2019/10/18 20:51:19 (permalink)
    0
    Use basic csp uart driver and not the core one.
    Go check harmony docs for csp uart at ...HarmonyFramework\csp\doc
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5