• AVR Freaks

Hot!Looking for an 8-bit MCU with minimum 5 UART peripheral ports

Author
naeem1234
Super Member
  • Total Posts : 451
  • Reward points : 0
  • Joined: 2015/02/19 06:39:28
  • Location: 0
  • Status: offline
2019/10/12 23:54:02 (permalink)
0

Looking for an 8-bit MCU with minimum 5 UART peripheral ports

Hello
 
I am looking for an MCU that has min 5 (or maybe more) UART ports in the hardware. How can I search for this?
#1

3 Replies Related Threads

    1and0
    Access is Denied
    • Total Posts : 10294
    • Reward points : 0
    • Joined: 2007/05/06 12:03:20
    • Location: Harry's Gray Matter
    • Status: offline
    Re: Looking for an 8-bit MCU with minimum 5 UART peripheral ports 2019/10/13 00:34:38 (permalink)
    +1 (1)
    naeem1234 
    I am looking for an MCU that has min 5 (or maybe more) UART ports in the hardware. How can I search for this?

    https://www.microchip.com/maps/Microcontroller.aspx
     
    #2
    ric
    Super Member
    • Total Posts : 25483
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: Looking for an 8-bit MCU with minimum 5 UART peripheral ports 2019/10/13 00:45:40 (permalink)
    +1 (1)
    When you use the abive link, you will discover that there are only three PIC parts, and 20 AVR parts with enough UARTs.
    The big question is, do you need to be communicating on all 5 ports simultaneously?
    If not, then a part with one or two UARTs and a PPS peripheral may well be adequate.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #3
    ALostCause12
    New Member
    • Total Posts : 5
    • Reward points : 0
    • Joined: 2019/08/28 13:14:02
    • Location: 0
    • Status: offline
    Re: Looking for an 8-bit MCU with minimum 5 UART peripheral ports 2019/10/30 11:52:24 (permalink)
    0
    @ric is correct - you can see an example of how to do this in TB3151 (http://ww1.microchip.com/downloads/en/Appnotes/90003151A.pdf) which shows something similar but with the MSSP peripheral and even includes some example code. 
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5