• AVR Freaks

Harmony 3 Help & PWM Disable

Author
WoSta
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/10/08 04:50:24
  • Location: 0
  • Status: offline
2019/10/10 23:42:33 (permalink)
0

Harmony 3 Help & PWM Disable

Hy,
 
Till shortly i was useing harmony 2 and there was a great help tool in the install folder of harm2. All functions like "ChannelPWMxHDisable" where discibed very good.
Does anybody knew if there is the same tool in Harm 3.
Does anybody knew how i can disable a single PWM channel with harm3 ?
 
thx
greetings wolfgang
#1

1 Reply Related Threads

    yts
    Super Member
    • Total Posts : 599
    • Reward points : 0
    • Joined: 2005/09/06 17:45:30
    • Status: offline
    Re: Harmony 3 Help & PWM Disable 2019/10/11 19:35:16 (permalink)
    0
    For example, the function
    void OCMP4_Disable (void)
    is in plib_ocmp4.c.
     
    yts
    post edited by yts - 2019/10/11 19:45:57

    Attached Image(s)

    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5