• AVR Freaks

PIC32MX360 and Serial communication

Author
polinag96
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/10/02 11:22:31
  • Location: 0
  • Status: offline
2019/10/10 07:36:40 (permalink)
0

PIC32MX360 and Serial communication

I am trying to use a simple USART tutorial code https://microchipdeveloper.com/harmony:example-usart-dynamic-wf32 on my PIC32MX360 starter kit just to test run serial however, my PIC isn't recognized as a serial (com) port. It shows up as a high speed USB and I can't run my outputs on a serial terminal. Can anyone help? I am new at this. I am using a mac.
#1

3 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 17847
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: PIC32MX360 and Serial communication 2019/10/10 18:40:02 (permalink)
    0
    Huh?  This is to connect you PIC to a serial Port. 
    Are you connecting it to a USB Port and expectiong it to enumerates as a CDC Device (serial Port)?
    #2
    ric
    Super Member
    • Total Posts : 23886
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: PIC32MX360 and Serial communication 2019/10/10 19:19:50 (permalink)
    0
    As above.
    USART ≠ CDC
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #3
    ric
    Super Member
    • Total Posts : 23886
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: offline
    Re: PIC32MX360 and Serial communication 2019/10/10 19:24:03 (permalink)
    0
    I suspect you totally skipped over the second paragraph of that tutorial...

    The hardware for this project uses the chipKIT® WF32 board from Digilent® Inc. This board uses an FTDI USB to UART converter, which connects to the USART1 TX and RX pins (U1TX, U1RX) on the PIC32.


    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #4
    Jump to:
    © 2019 APG vNext Commercial Version 4.5