• AVR Freaks

Harmony V3 Change notification interrupt not triggering (SOLVED)

Author
MantasP
New Member
  • Total Posts : 15
  • Reward points : 0
  • Joined: 2019/02/20 03:31:39
  • Location: 0
  • Status: offline
2019/10/10 04:21:00 (permalink)
0

Harmony V3 Change notification interrupt not triggering (SOLVED)

Hi I'm trying to setup a change notification for a pin on pic32mz ef starter kit. 

I have selected the CN enable on the pin configurator and the cn interrupt is also enabled in the system -> pic32mz interrupts menu.
 
void CHANGE_NOTICE_D_Handler (void)
{
CHANGE_NOTICE_D_InterruptHandler();
}

The handler is never called when I change the state of the pin. Anyone got this working with harmony 3 configurator?
post edited by MantasP - 2019/10/10 04:42:14
#1

1 Reply Related Threads

    MantasP
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2019/02/20 03:31:39
    • Location: 0
    • Status: offline
    Re: Harmony V3 Change notification interrupt not triggering 2019/10/10 04:42:00 (permalink)
    4 (1)
    OK need to add this 

    GPIO_PortInterruptEnable(GPIO_PORT_D, 0x01);
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5