• AVR Freaks

Missing function?

Author
Szuszu
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/08/02 01:23:24
  • Location: 0
  • Status: offline
2019/10/09 06:41:57 (permalink)
0

Missing function?

hi,
 
I want to use a checkbox in may app and query it's state (checked, unchecked), but laCheckBoxWidget_GetChecked function seems broken.
In libaria_widget_checkbox.h can found this: LIB_EXPORT laBool laCheckBoxWidget_GetChecked(laCheckBoxWidget* cbox);
...but in .c file has no contains the necessery routin.
 
or is it normal??
 
The debugger gives error: ...undefined reference to `laCheckBoxWidget_GetChecked'
 
if (laCheckBoxWidget_GetChecked(cb_DHCPon)) {
laCheckBoxWidget_SetChecked(cb_DHCPon, LA_FALSE);
} else {
laCheckBoxWidget_SetChecked(cb_DHCPon, LA_TRUE);
}
 
thanks your help
#1

0 Replies Related Threads

    Jump to:
    © 2019 APG vNext Commercial Version 4.5