• AVR Freaks

dsPIC33CHxxxMPxxx Parallel Master Port (PMP)

Author
Björn
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2018/01/08 08:07:53
  • Location: 0
  • Status: offline
2019/10/07 05:56:43 (permalink)
0

dsPIC33CHxxxMPxxx Parallel Master Port (PMP)

Hello,
i want to upgrade a project from a PIC24FJ64GA004 to a dsPIC33CH512MP205.
In the Parametric Search the PMP is listed as a feature, but i can't find anything in the datasheet about it.
Is it listed incorrectly or am i looking for the wrong thing in the datasheet? Is it called different there?
Has anyone used this family with the PMP before?
post edited by Björn - 2019/10/07 05:59:43
#1

2 Replies Related Threads

    Gort2015
    Klaatu Barada Nikto
    • Total Posts : 3292
    • Reward points : 0
    • Joined: 2015/04/30 10:49:57
    • Location: 0
    • Status: offline
    Re: dsPIC33CHxxxMPxxx Parallel Master Port (PMP) 2019/10/07 06:40:40 (permalink)
    0
    It's not supported, everything is serial but you can still use the Ports for parallel comms.

    MPLab X playing up, bug in your code? Nevermind, Star Trek:Discovery will be with us soon.
    https://www.youtube.com/watch?v=Iu1qa8N2ID0
    + ST:Continues, "What Ships are Made for", Q's back.
    #2
    spdmtl
    New Member
    • Total Posts : 16
    • Reward points : 0
    • Status: offline
    Re: dsPIC33CHxxxMPxxx Parallel Master Port (PMP) 2019/10/10 08:41:27 (permalink)
    0
    The single core version, dsPIC33CK256MP508 family has the PMP. 
    #3
    Jump to:
    © 2019 APG vNext Commercial Version 4.5