• AVR Freaks

Helpful ReplyHot!Is there a way to limit total programming counts on pickit3?

Author
seyyah
Super Member
  • Total Posts : 633
  • Reward points : 0
  • Joined: 2004/05/14 12:49:28
  • Status: offline
2019/10/02 03:32:46 (permalink)
0

Is there a way to limit total programming counts on pickit3?

I want to program my boards on the field using pickit 3 programmer to go function(or may be pickit 4 which I did not try yet). I sometimes require it to give somebody else for some purpose. In that case I want to limit its usage to a certain number of programmings. For example it should allow 10 boards to program and not beyond it. Is there a way to do it? Thanks.
#1
NorthGuy
Super Member
  • Total Posts : 6169
  • Reward points : 0
  • Joined: 2014/02/23 14:23:23
  • Location: Northern Canada
  • Status: offline
Re: Is there a way to limit total programming counts on pickit3? 2019/10/02 05:46:41 (permalink) ☄ Helpfulby seyyah 2019/10/07 01:44:35
5 (1)
If you want to do this because you're afraid that they may steal your firmware, one programming is enough to do this.
#2
seyyah
Super Member
  • Total Posts : 633
  • Reward points : 0
  • Joined: 2004/05/14 12:49:28
  • Status: offline
Re: Is there a way to limit total programming counts on pickit3? 2019/10/02 13:08:09 (permalink)
0
No I don't fear of stealing. More like I want to know howmany time the program is used which will be reported literally but as a safeguard to limit it to a value to make certain it will return to me ultimately.
#3
NKurzman
A Guy on the Net
  • Total Posts : 18779
  • Reward points : 0
  • Joined: 2008/01/16 19:33:48
  • Location: 0
  • Status: offline
Re: Is there a way to limit total programming counts on pickit3? 2019/10/02 14:47:24 (permalink) ☄ Helpfulby seyyah 2019/10/07 01:44:38
5 (1)
Since no one said Yes, then the Answer may be no.  I know there are other 3rd party ones that do limit the number of writes.
If you concern is getting it back go with the core charge.  Return it in 30 days or you will be charged.  Or Pay first and refund on return.
#4
rths
New Member
  • Total Posts : 2
  • Reward points : 0
  • Status: offline
Re: Is there a way to limit total programming counts on pickit3? 2019/10/11 22:57:13 (permalink)
0
Hi Seyyah,
Maybe, through Pk3/pk4 we can't control the programming count but we can control through PM3. In PM3 using SQTP we can control the programming count.
#5
Jump to:
© 2020 APG vNext Commercial Version 4.5