• AVR Freaks

Hot!Sitronix ST7701 LCD controller

Author
i4cy
New Member
  • Total Posts : 27
  • Reward points : 0
  • Joined: 2014/03/25 05:22:23
  • Location: 0
  • Status: offline
2019/09/26 01:57:16 (permalink)
0

Sitronix ST7701 LCD controller

Does Harmony or will it support in the near future the Sitronix ST7701 LCD controller?
 
Segger emWin supports other Sitronix displays like ST7712, ST7715, ST7735, ST7789, ST7796 using the GUIDRV_FlexColor driver. Are these displays architecturally similar enough so that the GUIDRV_FlexColor driver can be used with the ST7701?
 
Thanks.
post edited by i4cy - 2019/09/26 02:02:00
#1

1 Reply Related Threads

    i4cy
    New Member
    • Total Posts : 27
    • Reward points : 0
    • Joined: 2014/03/25 05:22:23
    • Location: 0
    • Status: offline
    Re: Sitronix ST7701 LCD controller 2019/10/10 07:26:07 (permalink)
    0
    To answer my own question...
     
    ST7701 is not similar to the other displays, but the GUIDRV_Lin driver can be used.
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5