• AVR Freaks

Hot!code model size

Author
daverj
Starting Member
  • Total Posts : 58
  • Reward points : 0
  • Joined: 2011/03/26 12:47:21
  • Location: 0
  • Status: offline
2019/09/21 20:10:14 (permalink)
0

code model size

I've updated from MPLABX 3.15 to 5.25, and XC16 1.25 to 1.41 and am compiling an old project that I want to migrate to the new environment. But something is confusing me. While compiling the project, in the middle of the output listing it says:
 
xc16-ld 1.41 (A)

Default Code Model: Small
Default Data Model: Large
Default Scalar Model: Small


I have Code Model set to "Large" in the project properties. Is this just telling me what the default sizes would be if I were to select "Default" in the project properties? Or is it somehow overriding my setting for Code Model size?
 
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5