• AVR Freaks

Hot!library differences from 1.25 to 1.41

Author
daverj
Starting Member
  • Total Posts : 58
  • Reward points : 0
  • Joined: 2011/03/26 12:47:21
  • Location: 0
  • Status: offline
2019/09/21 15:45:42 (permalink)
0

library differences from 1.25 to 1.41

I have a project I wrote a couple of years ago with XC16 v1.25.
 
The microchip/XC16/v1.25/lib folder contained folders for each series (ie: PIC24E) and within those were libraries for each part, such as: "libp24ep512gp204-elf.a"
 
In my old project I copied that file into the project and linked it in.
 
In the v1.41/lib folder there are no such folders for the separate series of parts, with libraries for individual parts. Since this was a few years ago I don't remember what specifically I was using that required me to link in that specific library. What library am I supposed to use instead, now that I'm compiling with XC16 v1.41?
#1

2 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 18672
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: library differences from 1.25 to 1.41 2019/09/21 17:54:18 (permalink)
    0
    The old PLIB libraries are discontinued.
    They are available as a separate download, but may not work with the new were compilers. You can still download an older version of the compiler if you need to build an old project.
    #2
    mpgmike
    Super Member
    • Total Posts : 420
    • Reward points : 0
    • Joined: 2014/01/23 17:27:06
    • Location: NJ
    • Status: offline
    Re: library differences from 1.25 to 1.41 2019/09/22 18:08:47 (permalink)
    0
    You should find that all you need is:

    # include <xc.h>


    I don't need the world to know my name, but I want to live a life so all my great-grandchildren proudly remember me.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5