• AVR Freaks

Hot!How to use CDC on PIC18F47K42 Curiosity Nano

Author
ThoWa
New Member
  • Total Posts : 11
  • Reward points : 0
  • Joined: 2019/08/23 23:45:40
  • Location: 0
  • Status: offline
2019/09/21 13:50:31 (permalink)
0

How to use CDC on PIC18F47K42 Curiosity Nano

I'm wondering to to use the CDC on curiosity nano board to Transfer data between  PC and the target.
According to Pinout in Figure 4-1 of PIC18F47K42-Curiosity-Nano-User-Guide-50002899A.pdf the Pins RD0 and RD1 should supply TX and RX, but in Pin Manager Grid View I cannot set those PINs to UART1.
 
post edited by ThoWa - 2019/09/21 13:53:30

Attached Image(s)

#1

2 Replies Related Threads

    ThoWa
    New Member
    • Total Posts : 11
    • Reward points : 0
    • Joined: 2019/08/23 23:45:40
    • Location: 0
    • Status: offline
    Re: How to use CDC on PIC18F47K42 Curiosity Nano 2019/09/21 14:21:21 (permalink)
    0
    I figured out, after adding UART2 to my Project in Resource View I could assing RD0 and RD1 ;-)
     
    #2
    davekw7x
    Entropy++
    • Total Posts : 1870
    • Reward points : 0
    • Joined: 2012/01/16 12:01:07
    • Location: Second star on the right, straight on till morning
    • Status: offline
    Re: How to use CDC on PIC18F47K42 Curiosity Nano 2019/09/21 14:45:06 (permalink)
    0
    Redundant narrative deleted by davekw7x
     
    The OP found the problem while I was crafting a reply telling the same thing.
     Sorry.  Didn't mean to step on your toes.
     
    Regards,

    Dave
    post edited by davekw7x - 2019/09/21 17:02:31

    Attached Image(s)


    Sometimes I just can't help myself...
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5