• AVR Freaks

Hot!h

Author
ptajay
New Member
  • Total Posts : 8
  • Reward points : 0
  • Joined: 2019/06/30 21:28:57
  • Location: 0
  • Status: offline
2019/09/20 21:58:50 (permalink)
0

h

.
post edited by ptajay - 2019/10/15 06:37:38
#1

2 Replies Related Threads

    ric
    Super Member
    • Total Posts : 27057
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: Help With Generating PWM using Interrupt using PIC32MZ harmony 2019/09/21 04:43:18 (permalink)
    0
    Do you need to update the PWM duty cycle on every single cycle?
    Normally you can set PWM and it will maintain itself until you need to update it.
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    ptajay
    New Member
    • Total Posts : 8
    • Reward points : 0
    • Joined: 2019/06/30 21:28:57
    • Location: 0
    • Status: offline
    Re: Help With Generating PWM using Interrupt using PIC32MZ harmony 2019/09/21 04:57:31 (permalink)
    0
    yes...I need to update PWM every cycle and I am trying to change the duty reg value to be written in OC1RS in the interrupt of the OC. Is this possible? if so how?
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5