• AVR Freaks

AnsweredHot!Where is download of a separate stand-alone Harmony-3 executable?

Author
bird
Starting Member
  • Total Posts : 15
  • Reward points : 0
  • Joined: 2018/02/05 20:04:20
  • Location: 0
  • Status: offline
2019/09/19 20:12:45 (permalink)
0

Where is download of a separate stand-alone Harmony-3 executable?

Harmony main page states that Harmony-3
"Available as a plug-in that directly integrates with MPLAB X IDE and as a separate Java executable for stand-alone use"
But I can't find a link to stand-alone version. Git pages also do not show link to this download. Does it exist?
#1
nigelwright7557
Super Member
  • Total Posts : 427
  • Reward points : 0
  • Joined: 2006/11/06 08:15:51
  • Location: 0
  • Status: offline
Re: Where is download of a separate stand-alone Harmony-3 executable? 2019/09/19 20:17:22 (permalink)
0
I didn't know it could be stand alone.
If you are going to use Harmony then its usually as part of MPLAB X.
Harmony creates the code and MPLAB X XC compiler compiles it.
#2
bird
Starting Member
  • Total Posts : 15
  • Reward points : 0
  • Joined: 2018/02/05 20:04:20
  • Location: 0
  • Status: offline
Re: Where is download of a separate stand-alone Harmony-3 executable? 2019/09/19 23:18:56 (permalink)
0
The quote I provided about stand-alone Harmony 3 is taken from the Harmony main page
 https://www.microchip.com/mplab/mplab-harmony
and also
https://microchip-mplab-harmony.github.io/
if it is true such version exists and could be run with JVM, then
I want to run stand-alone version to verify if the problem of failing DB generation will be repeated there or is it only showing in MPLAB...
#3
JPortici
Super Member
  • Total Posts : 1021
  • Reward points : 0
  • Joined: 2012/11/17 06:27:45
  • Location: Grappaland
  • Status: offline
Re: Where is download of a separate stand-alone Harmony-3 executable? 2019/09/20 00:28:35 (permalink) ☼ Best Answerby bird 2019/09/20 19:09:15
0
I didn't know either until yesterday.
 
Go to your harmony 3 installation folder. Inside the MHC folder there are a bunch of JAR files.
 
harmony downloader is (obviously) the downloader. Huge time saver.
Hugely embarassing that this software takes 250MB or ram while doing nothing
 
runmhc.bat will launch mhc.jar with the correct parameters to run it standalone.
Another time saver as it will run on a different thread than MPLAB X (which is still single thread).
 
Enjoy :)
#4
bird
Starting Member
  • Total Posts : 15
  • Reward points : 0
  • Joined: 2018/02/05 20:04:20
  • Location: 0
  • Status: offline
Re: Where is download of a separate stand-alone Harmony-3 executable? 2019/09/20 19:09:16 (permalink)
0
Thank you JPortini, indeed runmhc.bat launched configurator and I opened "harmony.prj" and got all the configuration screens for the same project which failed in MPLAB ( Java threw exception and *.jar object failed to be created) .
Apparently the problem is within MPLAB environment only.
Thanks again - this is useful to know.
post edited by bird - 2019/09/20 19:14:01
#5
Jump to:
© 2020 APG vNext Commercial Version 4.5