• AVR Freaks

Hot!How to program pic32MK family without downloading MPLABX

Author
shmak
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/05/01 08:38:19
  • Location: 0
  • Status: offline
2019/09/17 16:48:07 (permalink)
0

How to program pic32MK family without downloading MPLABX

I tried using the scripting tool found in an archive for pickit3 programmers. This is not ideal because 1) It does not seem to recognize newer programmers like pickit4 and icd4 2) the programming app does not seem to recognize the pic32MK family. The README suggests that it supports the pic32mx family but even those devices do not show on the device pull down menu. 
 
Is there a better alternative solution. I want a quick and simple way to program hex files onto pic32mk motor control mcus. 
#1

2 Replies Related Threads

    ric
    Super Member
    • Total Posts : 25139
    • Reward points : 0
    • Joined: 2003/11/07 12:41:26
    • Location: Australia, Melbourne
    • Status: online
    Re: How to program pic32MK family without downloading MPLABX 2019/09/17 17:02:02 (permalink)
    0
    Do you really mean without DOWNLOADING MPLABX, or just without RUNNING MPLABX?
    MPLABX comes with a command line programming tool named "MPLAB X IPE". You can use that to access all the programmers and program all the latest chips. You do have to download and install MPLABX to get it, but you don't have to run MPLABX.
     
     

    I also post at: PicForum
    Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
    NEW USERS: Posting images, links and code - workaround for restrictions.
    To get a useful answer, always state which PIC you are using!
    #2
    newfound
    Super Member
    • Total Posts : 1849
    • Reward points : 0
    • Joined: 2003/11/07 12:35:49
    • Status: offline
    Re: How to program pic32MK family without downloading MPLABX 2019/09/17 17:09:56 (permalink)
    0
    Don't know of many options but here is one: https://www.northernsoftware.com/ 
     
    There is also the "microbridge" https://geoffg.net/microbridge.html but it is exceptionally slow and only really useful for very occasional updates. 
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5