• AVR Freaks

Hot!Sigma Delta ADC

Author
NICK7
Starting Member
  • Total Posts : 45
  • Reward points : 0
  • Joined: 2006/04/15 03:40:32
  • Location: 0
  • Status: offline
2019/09/15 22:31:28 (permalink)
0

Sigma Delta ADC

Hi
my configuration :
MPLAX v5.25
JAVA 1.8.0.181
WIN10
CCC 3.85.1
PIC24FJ128GC006T-I/PT
 
when I make changes to SDADC configuration window and then press generate nothing happens. On the contrary other module changes cause generate button to trigger merger ....etc.
 
Regards Nick
#1

1 Reply Related Threads

    pr.mchp
    Starting Member
    • Total Posts : 39
    • Reward points : 0
    • Joined: 2015/03/23 06:20:48
    • Location: 0
    • Status: offline
    Re: Sigma Delta ADC 2019/09/17 20:14:54 (permalink)
    0
    If there are no user changes(manually done) in the driver code, there will not be a trigger to the merger window for that module, when generate button is pressed after making changes in the UI the next time. A auto merge would happen for the changes made in the UI.
    #2
    Jump to:
    © 2020 APG vNext Commercial Version 4.5