• AVR Freaks

AnsweredHot!Debugging DM164143

Author
bena
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/09/13 03:26:43
  • Location: 0
  • Status: offline
2019/09/14 01:15:52 (permalink)
0

Debugging DM164143

Hi, is it possible to debug the PIC16F15376 on this XPress board(https://www.microchip.com/DevelopmentTools/ProductDetails/PartNo/DM164143)?
I can drag and drop all kinds of programs but I haven't been able to find any information that says how to step through code for it.
#1
ric
Super Member
  • Total Posts : 27057
  • Reward points : 0
  • Joined: 2003/11/07 12:41:26
  • Location: Australia, Melbourne
  • Status: online
Re: Debugging DM164143 2019/09/17 17:49:13 (permalink)
0
Haven't tried it, but this page says you have some simplified debugging in the Express IDE
https://microchipdeveloper.com/xpress:xpressdebug
 

I also post at: PicForum
Links to useful PIC information: http://picforum.ric323.co...opic.php?f=59&t=15
NEW USERS: Posting images, links and code - workaround for restrictions.
To get a useful answer, always state which PIC you are using!
#2
bena
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2019/09/13 03:26:43
  • Location: 0
  • Status: offline
Re: Debugging DM164143 2019/09/18 02:40:07 (permalink)
0
I tried to use it but it only uses the simulator. The debug tool is listed as "Simulator/Xpress Board".
The video at the bottom of the link shows that they're using a different type of Xpress board that uses "Curiosity" as its Debug tool. 
#3
Jams100001
Junior Member
  • Total Posts : 78
  • Reward points : 0
  • Joined: 2018/04/12 13:37:33
  • Location: MCHP Chandler
  • Status: offline
Re: Debugging DM164143 2019/10/07 09:35:42 (permalink) ☼ Best Answerby bena 2019/10/10 02:40:16
5 (1)
Ben,
The DM164143 was never designed to be a debugger.  You can get a DM164148 which is called a PIC16F15376 Curiosity Nano you will be able to debug with it. The price is relatively reasonable.
Jamus
#4
Jump to:
© 2020 APG vNext Commercial Version 4.5